Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
My contact person
Select location
NZ(EN)
Predictive
maintenance
FAQ
Ask your own question here

Predictive maintenance: definition, benefits, examples ... all with one click!

All questions and answers regarding predictive maintenance with igus® - smart plastics

Question after question - and we provide the answers! Here, you will find a summary of everything regarding predictive maintenance, sorted by topic and answered specifically. Immerse yourself in the world of predictive maintenance and let the advantages of our smart plastics technology convince you.

Maintenance strategies

Other maintenance strategies

Further materials

More materials on predictive maintenance

General information on predictive maintenance

General

► What is predictive maintenance?

Predictive maintenance is generally understood to mean the early anticipation and avoidance of an error in machinery or components thanks to data on their condition. This is possible with data-based methods that analyse the condition of your machines and help predict malfunctions, faults and also the time when maintenance work is required.

► What is the relationship between predictive maintenance and Industry 4.0?

Industry 4.0 promises greater efficiency in production through networked machines, insights due to data analyses and better machine availability. In this context, predictive maintenance, i.e. a forward-looking maintenance process based on the evaluation of process and machine data, is a crucial component. 

► What is the goal of predictive maintenance?

Unplanned downtime of production equipment costs money and cuts your profits significantly in the long run. What is certain is that machine and system failures pose a serious threat to the industrial sector. Predictive maintenance is intended to lead to cost savings compared to routine, interval- or time-based preventive maintenance as work is only carried out when necessary.

► What do I need to use predictive maintenance?

First of all, you need various sensors to record functionally relevant data on the machines, such as speed, temperature, noise level, bearing vibrations or power consumption. After that, a combination of real-time analysis technology and a database is required for the interpretation and meaningful evaluation of the sensor data. If all this is successful, it will be possible to fix the machine problem before it actually arises.

► Is predictive maintenance only suitable for conventional MRO companies?

No; predictive maintenance is not only interesting for the manufacturing industry or associated MRO areas (maintenance, repair and operations), but also for all mobility offers - be it in the air, in vehicles or on rails. It is usually worthwhile for companies that use the same type of machine more often or that do not want to use predictive maintenance for their own production but for the machines they sell.


Advantages of predictive maintenance

► What are the advantages of predictive maintenance?

The advantages and added values for companies can be quickly summarised:
  • Higher availability of the systems due to less downtime
  • Maximisation of plants' and machines' service life
  • Optimised deployment of maintenance technicians
  • Scheduled maintenance time
  • Higher machine performance and productivity
► Apart from the obvious advantages of predictive maintenance, are there also disadvantages?

There are, of course, the one-time investment costs in sensor hardware and software for data analysis and evaluation. In addition, every new method means initial change and training costs. With the ready-to-install smart plastics solutions from igus i.Cee, however, these can be reduced to a minimum.  
► What savings potential can be achieved with predictive maintenance?

Between 50 and 70% less unplanned downtime should be possible as well as savings of 20 to 40% maintenance costs - depending on which study by the two renowned consulting firms McKinsey or Accenture you prefer to trust. In addition, Roland Berger claims to have discovered that with predictive maintenance, only 15% of the time is spent on maintenance, compared to 40% with conventional reactive maintenance.
► Does predictive maintenance also improve OEE (overall equipment effectiveness)?

According to the authors of a survey that Bearing Point, another technology consultancy, conducted among experts in maintenance, production, logistics and IT, over 80% of users expect predictive maintenance to increase plant availability, i.e. OEE. 

Requirements for predictive maintenance

► How can I get started with predictive maintenance right away?

The collection and analysis of machine data is essential for this type of intelligent maintenance work. With the help of the data, it is possible to calculate the optimum time for maintenance so as to avoid disruptions. Machine data is usually collected via sensors attached to the machine or plant component, often appropriately referred to as predictive maintenance sensors. With the igus energy chains, this task is carried out by the i.Sense condition monitoring sensors from smart plastics. This smart sensor technology continuously records the various operating states of the energy supply.
► What other data is needed to get a maintenance forecast that is as accurate as possible?

The prerequisite for an accurate indication of the trouble-free operation time is that information on use is as precise as possible. This includes information about the operation site with weather conditions and temperatures, travel distances, number of cycles etc. Thanks to the knowledge acquired in the igus test laboratory and the current status data, igus is able to precisely predict the life data. The necessary replacement of a component is then displayed in good time and enables scheduled and resource-conserving maintenance.
► Do you always need new software or a new IT tool for predictive maintenance?

The prerequisite for predictive maintenance is that the machines are networked, i.e. all machines provide their data in a database for storage and analysis. This is mostly carried out with an OPC UA protocol. However, with the igus i.Cee solutions for predictive maintenance, no additional systems or hardware are required. All necessary data is provided via the associated i.Sense sensors, and the special AI algorithms are implemented in the i.Cee module. The associated i.Cee dashboard can be accessed with any ordinary PC.
The diagram shows the importance of i.Sense as predictive maintenance sensors for i.Cee. The diagram shows the importance of i.Sense as predictive maintenance sensors for i.Cee.

Application areas of predictive maintenance

► What examples of predictive maintenance are there in practice?

In practice, it often makes sense to use predictive maintenance with machines where a breakdown would mean high sales losses or consequential damage. Modern machines are often already equipped with the necessary measuring sensors, older ones can be retrofitted. Here are a few examples: 

  • Vibration measurements on systems provide information about imbalances, incipient bearing damage etc.
  • Temperature measurement systems provide information about bearing damage or cooling problems.
  • Measurements of the power consumption of pumps, motors etc. indicate sluggish drives, couplings etc.
  • Measurements of the transmission properties of data cables shed light on the remaining service life.
  • Force or load cell sensors help determine the current utilisation.
In the field of dynamic energy supply applications, igus already offers a wide product range with its smart plastics.
 

► In which industries does predictive maintenance make the most sense?

Predictive maintenance is primarily used in industries in which the failure of systems, machines or components means significant consequential damage and failure costs:

  • Aviation: airlines use sensors in their machines to replace wear-resistant parts, such as turbines or pumps, in good time and to avoid downtime on the ground. 
  • Automotive: automotive companies operate some of the largest robot fleets in the world, produce just in time and have tightly integrated supply chains. Any problem in production, such as an unplanned downtime, disrupts the entire supply chain.
  • Wind turbines: today, vibration analyses can prevent failures of wind turbines almost entirely.
  • Ports: the failure of cranes means long waiting times for ships and less throughput for ports. 
In most of these industries, predictive maintenance solutions from igus - smart plastics are already in use. 
 

Other maintenance strategies

► What other maintenance strategies are there besides predictive maintenance?

In its DIN EN 13306, Terms of Maintenance, the Deutsches Institut für Normung e.V. (German Institute for Standardization) defines a maintenance strategy as a procedure for achieving maintenance goals, such as maintaining a specified condition or extending a machine's service life. A distinction is usually made between the following three different approaches:
  • Reactive maintenance strategy/damage-based maintenance strategy
  • Prophylactic maintenance strategy/preventive maintenance strategy
  • Anticipatory maintenance strategy/predictive maintenance strategy
► What characterises reactive maintenance?

With the reactive form of maintenance, damage to machines is repaired and production parts are replaced only when there is an acute problem. This means that companies have to react quickly in the event of damage in order to be able to continue production as quickly as possible and avoid high downtimes and costs. Most often, this strategy is used with machines that don't need to be repaired often or that can be repaired or replaced cheaply.
What is the difference between preventive and predictive maintenance?

Preventive maintenance is a maintenance strategy in which maintenance measures are carried out at specific intervals. The intervals can depend on time or quantity. This means that people don't wait for systems or machine parts to break down, but carry out systematic preventive inspections and maintenance measures. In this case, the actual degree of wear and tear of the machines and systems is not relevant. That procedure is in complete contrast to predictive maintenance: here, process and machine data is recorded during operation via sensors and interfaces, stored and then analysed.

Download more material

► Where can I find a summary of the most important information on predictive maintenance as a PDF or similar?

In our short guide on increasing machine availability (OEE), you will find all the details for further reading: 
► Where can I find a list of all igus offers on the subject of predictive maintenance:

You are welcome to take a look at all the available solutions directly in our igus online shop. 
► Where can I find an overview that not only covers predictive maintenance, but also condition monitoring?

In our smart plastics brochure, we give you a complete overview of the igus product portfolio for Industry 4.0. 

Information ...

News catalogue: 2022 smart plastics news Read everything about 2022 smart plastics news again in a compact PDF format.
News catalogue PDF

... Try it ...

smart 3D data Free 3D data, operating instructions, and much more in our smart plastics service area
3D data

... Realise

Buy smart plastics news in the igus online shop Order ready-to-install smart plastics directly in the igus online shop
Online shop


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH