Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
My contact person
Select location
NZ(EN)

Weighing and inspection technology

From the filling of packaging units to the positioning of cameras and sensors

In addition to high-precision weighing, modern multihead weighers are also capable of dosing and counting. Cameras and sensors are then used to check the quality of the packaging. In both places, lubrication-free and maintenance-free linear and rotary bearing technology is required, that enables long service life and meets the high FDA requirements.

About the individual stations and used materials


Weighing technology

At the heart of multihead weighers are the load cells with their high-precision measurement recordings. In addition to weighing, modern systems are also capable of dosing and counting. Requirements for the bearing technology used for this purpose include high precision, freedom from lubricants, corrosion resistance and resistance to cleaning agents.

Used products and application examples

The example of a Multipond multihead weighing system from Atoma GmbH shows two areas of application in which igus bearing products are used. Above all, igubal pillow block bearings, iglidur plain bearings and drylin linear bearings were installed here:

Ejection mechanism flap bearing

Filling/dosing

 
Atoma multihead weigher Atoma's Multipond multihead weighing systems can perform more than 500 weighings per minute with 36 heads.
Ejection mechanism flap bearing

Ejection mechanism flap bearing

iglidur plain bearings are used in the ejection mechanism of the containers. A single iglidur material is used universally for all weighing systems, which covers a wide temperature spectrum, is electrically conductive and meets the high hygienic standards.
Multihead weigher

Filling / Dosing

In the lowering screen drylin R linear bearings are used. The screen raises and lowers at a rapid rate and with a stroke of 40 millimetres above the packaging machine, enabling each individual packaging unit to be filled both quickly and precisely.

Inspection technology

In inspection technology, products go through various inspection processes that require the use of cameras and sensors. To ensure that these are moved precisely and reliably, suitable linear bearing technology must be found. Lubrication-free and FDA-compliant bearings are required, particularly in food packaging. In addition, the focus is on robust systems with long service life.

Used products and application examples

The TQS-SP TE system from Wipotec for testing and packaging products in folding boxes demonstrates the various requirements for bearing products within testing technology. In addition to format adjustments, the drylin lead screw linear systems used here are also used for the exact positioning of camera and sensor technology.

1. Side and format adjustment

2. Transfer roller

3. Side and height adjustment

4. Pressure roller

5. Positioning of sensors

6. Guide rollers
In the TQS-SP TE testing and packaging system from Wipotec, bearing products from our drylin and iglidur product portfolio prove themselves in the format adjustment.
Format adjustment

1. Side and format adjustment

drylin SHT linear systems with lead screw drive enable precise side and format adjustment by hand.
Transfer roller

2. Transfer roller

A highly wear-resistant round bar made of iglidur JB is used as a transfer roller in the system. It also offers low coefficient of friction and operates without lubrication.
Side and height adjustment

3. Side and height adjustment

The drylin lead screws used are robust and enable adjustment even under high loads and long stroke lengths.
Pressure roller

4. Pressure roller

Several pressure rollers are used for product transport, which keep the products securely on track and ensure the short processing cycles. In the rollers, lubrication and maintenance-free plain bearings made of iglidur J prove themselves, even in continuous operation.
Positioning of sensors

5. Positioning of sensors

In addition to the format adjustments of the testing and packaging unit, drylin SHT lead screw linear systems are also used for the adjustment of the sensors.
Guide rollers

6. Guide rollers

And last but not least, the module from Wipotec also uses xiros ball bearings in the guide rollers. Like all components, they are also FDA-compliant.

Customer application examples

Format adjustment in Krones test systems

Inspection technology machines from Krones rely on our plain bearings, slewing ring bearings, e-chains, gearbox solutions and linear axes for format adjustment.
Pneumatic flap control system

Pneumatic flap control system

In this weighing and filling system for food, the clevis joints are pneumatically controlled and thus actuate the flap system.

Testing and sorting plant

Testing and sorting plant

In this testing and sorting system, test parts are removed, measured and fed to various magazines with a vacuum gripper.
Filling and sealing machine

Filling and sealing machine

In addition to the high chemical resistance, the iglidur J plain bearings offer a maintenance-free dry operation in this application.

And many more ...

Discover even more successful applications in the beverage, food and packaging industries.

Consulting

I look forward to answering your questions

Shipping and consultation

In person:

Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.

Online:

24h


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH