Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
My contact person
Select location
NZ(EN)

Harnessed Single Pair Ethernet (SPE)

Simple and secure data communication to your plant

Digitisation and data exchange have become indispensable in modern production. With only one core pair in the Single Pair Ethernet, igus offers you the possibility of a guaranteed future data exchange. Transmission rates of up to 1GBit/s are easily possible and the minimisation of the cable to only one pair of cores offers you further advantages. You can use the 25% thinner cable compared to the CAT5e cable (CFBUS.PUR.045) in a confined installation space. It saves a lot of space, which has a great influence on dynamic motion sequences in the machinery.

The newly developed, industrial-grade plug-in connectors from Yamaichi and Weidmüller offer an excellent shield connection and thus reduce electromagnetic interference (EMC). The company igus offers a chainflex type with a highly abrasion-resistant and notch-resistant PUR outer jacket, which is sold by the metre. All ready-to-connect Single Pair Ethernet (SPE) cables are 100% tested by igus and thus ensure safe and reliable data communication.

Product extension 2023

Single Pair Ethernet new 2023
The company igus has been offering the harnessed SPE cable with Harting T1 connector since 2021. At the Hannover Messe 2023 we are expanding the range with two new, ready-to-connect, harnessed SPE cables. The new cables are available with plug-in connectors from Yamaichi and Weidmüller. For continuous industrial Ethernet communication in machines and systems with only one pair of cores for transmitting data. 

SPE with Yamaichi connector ► Buy online

SPE with Weidmüller connector ► Buy online
Tech up

Tech up

  • Energy chain-compatible Ethernet communication for the entire plant
  • 25% thinner than CAT5e, with the same data transmission rate
Cost down

Cost down

  • 25% smaller bend radius compared to CFBUS.PUR.045
  • Costs are 20% lower than those of a CAT5e cable (CFBUS.PUR.045)
  • Time saving as it is ready to connect
Proof

Proof

  • 100% digital and logic test incl. transmission speed (test seal and protocol)
  • Tested in the largest test laboratory of its kind for cables in moving applications
  • Member of the SPE Network
Sustainability

Sustainability

  • Future-proof data communication
  • Calculate guaranteed service life of the cable online

Product Manager Markus Hüffel will give a short introduction

Finally, the harnessed Single Pair Ethernet cable is available in addition to the version sold by the metre. Cable length and type of connector can be chosen freely, with no minimum order quantity.
SPE logo

The SPE Industrial Partner Network

igus continues to advance SPE together with strong partners

Single Pair Ethernet is the infrastructure foundation that makes IIoT and Industry 4.0 possible. In order to promote Single Pair Ethernet technology for the rapidly growing IIoT market, igus is participating in the SPE Industrial Partner Networks with established partners such as HARTING and TE Connectivity*. 

For the reliable establishment of the entire future SPE ecosystem, standards for transmission protocols, cabling and device components are also jointly developed and adopted and published in IEEE 802.3 and IEC SC46C. 

In this way, the new cable could also be constructed in partnership for the T1 connector interface. As a result, the durable shield has reliable transference to the connector, ensuring optimal high electromagnetic compatibility (EMC). The combination of chainflex cable and SPE connector is extremely robust: igus uses a highly abrasion-resistant, notch-resistant PUR jacket and the connector uses robust metallic interlocks with PCB socket.

* only valid for CAT9471001 with Harting T1 connector

Harnessed Single Pair Ethernet (SPE) in the product range

Part no. Outer jacket material Outer diameter (d) in mm Cable structure Bend radii Price
ready for shipping in 72 hours from stock Germany CAT9471001 PUR 5,5 (2x0,15)C 12,5 x d 136.47 NZD Add to shopping cart
ready for shipping in 72 hours from stock Germany CAT9471002 PUR 5,5 (2x0,15)C 12,5 x d 87.03 NZD Add to shopping cart
ready for shipping in 72 hours from stock Germany CAT9471003 PUR 5,5 (2x0,15)C 12,5 x d 92.67 NZD Add to shopping cart
More about selected part:
3D-CAD 3D-CAD
Sample request Sample request
Quote request Quote request
myCatalog myCatalog
Single Pair Ethernet all 3 types

To the shop for harnessed network technology

To the shop

Everything about the SPE (Single Pair Ethernet) cable

The key to industrial automation, the Industrial Internet of Things (IIoT)

Single Pair Ethernet technically describes the transmission of Ethernet (1000Base-T1) via only two pair of copper wires and enables both data transmission via Ethernet and simultaneous power supply (PoDL). This technological leap leads to a reduction of the diameter by approx. 25% compared to an ordinary Ethernet cable. This white paper gives an overview of the current state of development of SPE and shows the opportunities the new transmission technology opens up for the industry by significantly reducing the installation space as well as the associated weight reduction:
 

Up to 36 months chainflex guarantee

chainflex guarantee In addition to the SPE cables, we give a 36-month guarantee on all our chainflex cables in good faith, because with over 30 years of experience in our 3,800m² large test laboratory and 700 parallel running test trials, we can make reliable predictions about the service life of our cables.
Information here

Online shop for bus cables

Bus cable In addition to SPE, chainflex bus cables are also available for all other industrial bus systems such as Profinet, Ethernet, CAN bus or CC-Link. Depending on the cable family, they can be used for torsion resistance, tight radii, or particularly long travels and high speeds.
Buy here

Ready-to-connect cables

readycable portfolio Offering around 4,600 harnessed motor, servo, signal and encoder cables suitable for 24 manufacturer standards, igus is the world's No. 1 when it comes to harnessed cables for use in energy chains. With 7 cable qualities, we always offer the most cost-effective drive cable that works.
Click here


ready for shipping in 72 hours from stock Germany

The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH